RemoteConnect for the SCADAPack x70
Configuration & programming software application
Published by
Schneider Electric

RemoteConnect for the SCADAPack x70
Published by
Schneider Electric
Free
Features
Object database
User-defined names (tags):
Easily understood, relating directly to the process and/or equipment, and functionality RemoteConnect Object Browsers
Offline browser provides grouping, filtering, and sorting, for easy viewing and manipulation
Export/Import to/from Microsoft® Excel:
Facilitates external editing and templating of configurations to minimize engineering time, particularly for large systems
Protocol-agnostic:
Associate Modbus registers and/or DNP3 Level 4 objects with tagged database objects/variables
Optional DNP3 data concentrator Master for retrieval of DNP3 events and data
Modbus Scanner for configuration-based polling of Modbus devices without logic
Support for large object databases:
Up to 15000 objects
Up to 6000 logic-connected objects (included in the 15000 total)
X70 Logic editor
Share program sections with Modicon PLCs:
Logic code re-use between SCADAPack RTU and Modicon PLCs
Five IEC 61131-3 logic languages:
FBD – Function Block Diagram
LD – Ladder Diagram
SFC – Sequential Function Chart
IL – Instruction List
ST – Structured Text
Export/Import of logic program sections for reuse in other projects.
Cybersecurity
IP White List:
Restrict inbound & outbound comms. to specific IP addresses or ranges
Restrict communications to specific IP services or port numbers to limit access
DNP3 SAv2 Secure Authentication:
Authentication of critical commands over DNP3
Enable/Disable IP Services
Customer can choose which IP services to enable/disable and when, thus limiting cyber attack-surface exposure.
Third-party device management
RemoteConnect is an FDT2 Container
FDT2 –Field Device Tool, version 2
DTMs (High performance software drivers)
DTM -Device Type Manager
RemoteConnect accepts plug-in software DTMs of version 2 or version 1.2
Device DTMs are available from instrument vendors and provide an operator interface for managing and configuring the device
Communication DTMs provide the ‘protocol’ connection between the DTM and the device
Gateway DTMs act as a comms. bridge between networks and comm. DTMs
Customer can choose which IP services to enable/disable and when, thus limiting cyber attack-surface exposure.
Object database
User-defined names (tags):
Export/Import to/from Microsoft® Excel:
Protocol-agnostic:
Support for large object databases:
X70 Logic editor
Share program sections with Modicon PLCs:
Five IEC 61131-3 logic languages:
Export/Import of logic program sections for reuse in other projects.
Cybersecurity
IP White List:
DNP3 SAv2 Secure Authentication:
Enable/Disable IP Services
Third-party device management
RemoteConnect is an FDT2 Container
DTMs (High performance software drivers)