![](https://d2uars7xkdmztq.cloudfront.net/app_resources/77326/thumbs_112/img7873110828264208183.png)
Remote I/O IS1+ for EcoStruxure™ CPG
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/77326/thumbs_112/img7873110828264208183.png)
Remote I/O IS1+ for EcoStruxure™ CPG
Docs & Videos
Using M580 with Stahl Intrinsically Safe IO
The goal of this video is to show how easy is to configure Stahl Intrinsically safe I/O into a Modicon M580 system. The video will perform a Step-by-step integration of the Stahl Intrinsically safe I/O into a Modicon M580 PLC system. Stahl is a Schneider Electric CAPP Partner (Collaborative Automation Partner Program) and create solutions for Schneider Electric.
STAHL Remote I/O Systems - The Benchmark In Process Automation
Suited for diverse functions and the harshest of industrial environments, R. STAHL's Remote I/O systems are the ideal solution for your automation applications in the process industry.
IS1+ Remote I/O explained 1/3
With IS1+, R. STAHL presents a new I/O level that now can be applied even better and more effective. Explore the new functionalities and gain more information about our Remote I/O IS1+ modules in our informative video and on r-stahl.com/remoteio.
IS1+ Remote I/O explained 2/3
The new Remote I/O system IS1+ provides a range of interesting features and is more effective than ever before. Learn more about its architecture, interfaces and the supported protocols in this video and on r-stahl.com/remoteio.
IS1+ Remote I/O explained 3/3
Our Remote I/O IS1+ can be mounted and modified without the requirement for special engineering software, complicated regulations or tools.
IS1+ Remote I/O Explained | Industrial Automation | Digital Transformation
Our Senior Product Manager, André Fritsch answers FAQs about this future-proof technology. In this insightful video, he also shares his expert opinions on the advantages of IS1+ Remote I/O system in hazardous areas compared to conventional installations. Watch him as he talks about the cost-effectiveness, flexibility and the promising future of the IS1+ Remote IO technology.