![](https://d2uars7xkdmztq.cloudfront.net/app_resources/76729/thumbs_112/img1341503154736276149.png)
METRUM Manual Data Input Tool
Alternative WEB ETL for entering data into existing sources in PME through web app
Published by
METRUM
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/76729/thumbs_112/img1341503154736276149.png)
METRUM Manual Data Input Tool
Published by
METRUM
Overview
Enter data manually via the EcoStruxure™ Power Monitoring Expert web app
The first step for power management is to track all of your data. In situations where customers have an existing base of old devices it might be the case where we don´t have communication interfaces or the infrastructure won´t allow network connection. To allow these customers to give their first step in direction to power management, it is necessary to have ways for the data to be entered in PME, sometimes not automatically, and then be used in the same way as a direct connected source.
METRUM´s Manual Data Input Tool enable users with the right permissions to input data in PME´s Database directly through an embedded tab inside PME Web App interface.
Devices without communication
Production data
WAGES data
Finance data
Enter data manually via the EcoStruxure™ Power Monitoring Expert web app
The first step for power management is to track all of your data. In situations where customers have an existing base of old devices it might be the case where we don´t have communication interfaces or the infrastructure won´t allow network connection. To allow these customers to give their first step in direction to power management, it is necessary to have ways for the data to be entered in PME, sometimes not automatically, and then be used in the same way as a direct connected source.
METRUM´s Manual Data Input Tool enable users with the right permissions to input data in PME´s Database directly through an embedded tab inside PME Web App interface.
![Technology Partner](https://exchange.se.com/assets/img/technology-partners-certificate.jpg)