![](https://d2uars7xkdmztq.cloudfront.net/app_resources/76593/thumbs_112/img5291934007648734421.png)
EtherNet/IP to Profibus Gateway for Process Control and Asset Management
Integrate Profibus into EcoStruxure™ over EtherNet/IP
Published by
Softing Industrial Automation GmbH
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/76593/thumbs_112/img5291934007648734421.png)
EtherNet/IP to Profibus Gateway for Process Control and Asset Management
Published by
Softing Industrial Automation GmbH
Features
Quick gateway integration into engineering tool
Two workflows to integrate the epGate gateway in EcoStruxure™ Control Expert, either by using the generated EDS file (exported from the embedded Web server) or with the Schneider Electric Advanced Generic DTM (which is per default installed in EcoStruxure™ Control Expert).
Export of the *.XDB function blocks, used for data decoding in EcoStruxure™ Control Expert.
Asset management of Profibus field devices via FDT/DTM
Includes a communication Device Type Manager (CommDTM) for accessing Profibus field devices via FDT/DTM frame applications like Foxboro Field Device Manager (FDM) from Schneider Electric.
Access to technical support
First response provided within 2 working days.
Consulting & commissioning services are offered.
IoT Ready
Integration of MQTT and OPC UA interfaces for cloud applications.
Quick gateway integration into engineering tool
Two workflows to integrate the epGate gateway in EcoStruxure™ Control Expert, either by using the generated EDS file (exported from the embedded Web server) or with the Schneider Electric Advanced Generic DTM (which is per default installed in EcoStruxure™ Control Expert).
Export of the *.XDB function blocks, used for data decoding in EcoStruxure™ Control Expert.
Asset management of Profibus field devices via FDT/DTM
Includes a communication Device Type Manager (CommDTM) for accessing Profibus field devices via FDT/DTM frame applications like Foxboro Field Device Manager (FDM) from Schneider Electric.
Access to technical support
IoT Ready
Integration of MQTT and OPC UA interfaces for cloud applications.