OPC Server for Building Operations
Published by
Control See Ltd
Free Trial
Overview
OPC UA/DA Server for EcoStruxure™ Building Operation
The EBO-OPC server utilizes Schneider Electric’s SmartConnector system, to connect EBO (EcoStruxure™ Building Operation) data with any system that supports OPC (Open Platform Communications) client functionality.
Only when the value changes in the EBO system, is the information pushed by the EBO to the OPC server, and then to the OPC client system.
Most Building Management System (BMS), and SCADA systems support OPC client functionality, making the connection seamless.
Customers Testimonials
Equinix AM4 data center Amsterdam
"The EBO-OPC server was installed at the Equinix AM4 data center in Amsterdam. The EBO-OPC server enabled the customer to share EBO data with other OPC clients. Works as a charm!"
Chris Leijtens, Sr. System & Architecture Engineer - Europe Operations at Schneider Electric Netherlands.
OPC UA/DA Server for EcoStruxure™ Building Operation
The EBO-OPC server utilizes Schneider Electric’s SmartConnector system, to connect EBO (EcoStruxure™ Building Operation) data with any system that supports OPC (Open Platform Communications) client functionality.
Only when the value changes in the EBO system, is the information pushed by the EBO to the OPC server, and then to the OPC client system.
Most Building Management System (BMS), and SCADA systems support OPC client functionality, making the connection seamless.
Customers Testimonials
Equinix AM4 data center Amsterdam
"The EBO-OPC server was installed at the Equinix AM4 data center in Amsterdam. The EBO-OPC server enabled the customer to share EBO data with other OPC clients. Works as a charm!" Chris Leijtens, Sr. System & Architecture Engineer - Europe Operations at Schneider Electric Netherlands.