Smart Connector - AIDX
Connection between IATA - AIDX and EcoStruxure™ Building Operation
Published by
Schneider Electric

Smart Connector - AIDX
Published by
Schneider Electric
Overview
IATA - AIDX
Integration between EcoStruxure™ Building Operation and AIDX Flight Information Display System, is proposed to achieve energy efficiencies within the airport mechanical and electric systems. The solution optimises the run time and software control based on scheduled and actual events, occurring at the terminal gates.
By using a SmartConnector Extension to integrate these 2 platforms, information from the AIDX interface will be presented to an EWS Server, for EWS Clients such as EcoStruxure™ Building Operation to consume.
Aviation Information Data Exchange (AIDX) is the global XML messaging standard for exchanging flight data between airlines, airports, and any third party consuming the data. AIDX is endorsed as a standard by:
IATA Recommended Practice 1797A
ACI Recommended Practice 501A07
ATA Recommended Practice 30.201A
IATA - AIDX
Integration between EcoStruxure™ Building Operation and AIDX Flight Information Display System, is proposed to achieve energy efficiencies within the airport mechanical and electric systems. The solution optimises the run time and software control based on scheduled and actual events, occurring at the terminal gates.
By using a SmartConnector Extension to integrate these 2 platforms, information from the AIDX interface will be presented to an EWS Server, for EWS Clients such as EcoStruxure™ Building Operation to consume.
Aviation Information Data Exchange (AIDX) is the global XML messaging standard for exchanging flight data between airlines, airports, and any third party consuming the data. AIDX is endorsed as a standard by: