![](https://d2uars7xkdmztq.cloudfront.net/app_resources/118291/thumbs_112/image1861576811006107612.png)
Intesis ST Cloud Control Gateway for EcoStruxure™ Building Operation
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/118291/thumbs_112/image1861576811006107612.png)
Intesis ST Cloud Control Gateway for EcoStruxure™ Building Operation
Features
About Us
Intesis is a leader in designing, manufacturing, and commercializing innovative solutions for systems integration. Among these solutions, it provides the ST Cloud Control gateway.
ST Cloud Control provides a solution for managing buildings that do not fit into a traditional building automation system. With the increasing number of small buildings such as cell phone base stations and community centers, ST Cloud Control provides an affordable and efficient solution. With ST Cloud Control, customers can log in remotely using an app or web browser to control any BACnet or Modbus field devices on their buildings, making it easier to manage and make fast, impromptu changes to sites.
ST Cloud Technical Features
- Supports BACnet MS/TP & IP (one or the other) or Modbus RTU & TCP (simultaneously).
- Ethernet port for Cloud connectivity.
- 4/8/16/32 device management capability.
- MAPS configuration Tool.
- Android and iOS apps.
- Web-based dashboard for facility management and device sharing.
- 12 widgets/control variables per device.
- Templates for Schneider Electric’s field devices.
- BTL Certification that ensures interoperability with any BACnet devices.
ST Cloud General Features
- Leverages BACnet (IP & MSTP) and Modbus (TCP & RTU) as standards.
- Can work with any standard product independently of the manufacturer.
- Works with any size building.
- No programmers for API maintenance.
- Flexibility: ST Cloud Control supports parallel deployments with BMS.
Compatibility
ST Cloud Control device can communicate with any BACnet or Modbus standard devices. It opens multiple control capabilities within a building installation, from sensors to robust machinery, including UPS systems. It enables access to any Schneider Electric device remotely, reducing downtime, travel expenses and critical devices monitoring independently of the location, as long as the operator can use their mobile
phone or a web browser.
The capability to present any BACnet or Modbus device from a common dashboard brings many advantages in terms of compatibility with other manufacturers as well. While APIs requires development, maintenance, and support, using ST Cloud Control reduces the time to market and time expend with complex installation. Therefore, you can control building assets from any manufacturer, on multi-site installations, all using one common dashboard accessible from app or web.
About Us
Intesis is a leader in designing, manufacturing, and commercializing innovative solutions for systems integration. Among these solutions, it provides the ST Cloud Control gateway.
ST Cloud Control provides a solution for managing buildings that do not fit into a traditional building automation system. With the increasing number of small buildings such as cell phone base stations and community centers, ST Cloud Control provides an affordable and efficient solution. With ST Cloud Control, customers can log in remotely using an app or web browser to control any BACnet or Modbus field devices on their buildings, making it easier to manage and make fast, impromptu changes to sites.
ST Cloud Technical Features
- Supports BACnet MS/TP & IP (one or the other) or Modbus RTU & TCP (simultaneously).
- Ethernet port for Cloud connectivity.
- 4/8/16/32 device management capability.
- MAPS configuration Tool.
- Android and iOS apps.
- Web-based dashboard for facility management and device sharing.
- 12 widgets/control variables per device.
- Templates for Schneider Electric’s field devices.
- BTL Certification that ensures interoperability with any BACnet devices.
ST Cloud General Features
- Leverages BACnet (IP & MSTP) and Modbus (TCP & RTU) as standards.
- Can work with any standard product independently of the manufacturer.
- Works with any size building.
- No programmers for API maintenance.
- Flexibility: ST Cloud Control supports parallel deployments with BMS.
Compatibility
ST Cloud Control device can communicate with any BACnet or Modbus standard devices. It opens multiple control capabilities within a building installation, from sensors to robust machinery, including UPS systems. It enables access to any Schneider Electric device remotely, reducing downtime, travel expenses and critical devices monitoring independently of the location, as long as the operator can use their mobile phone or a web browser.
The capability to present any BACnet or Modbus device from a common dashboard brings many advantages in terms of compatibility with other manufacturers as well. While APIs requires development, maintenance, and support, using ST Cloud Control reduces the time to market and time expend with complex installation. Therefore, you can control building assets from any manufacturer, on multi-site installations, all using one common dashboard accessible from app or web.