![](https://d2uars7xkdmztq.cloudfront.net/app_resources/117921/thumbs_112/img1089925036059756903.png)
Intesis 700 Series Air Conditioner gateway for EcoStruxure™ Building Operation
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/117921/thumbs_112/img1089925036059756903.png)
Intesis 700 Series Air Conditioner gateway for EcoStruxure™ Building Operation
Docs & Videos
Intesis 700 Series Product Overview
This application series enables multiple connectivity options that are available from the same gateway platform. With the configuration tool MAPS, users can define the AC brand and protocol integration according to the project's needs.
A groundbreaking concept for HVAC integration
Intesis has recently launched the 700 Series Air, a groundbreaking concept that combines interfaces for multiple HVAC Brands and Building Automation protocols in the same hardware. This new product enables users to pair different combinations of HVAC brands and protocols using the Intesis MAPS configuration tool, a process called late configuration.
Setup Late Configuration on the 700 Series Air
Learn how to change the firmware of your 700 Series AC gateway with Intesis MAPS and locate the wiring diagram to wire the gateway correctly.