SCADAPack Workbench and Utilities
SCADAPack Programming Language Suite
Published by
Schneider Electric

SCADAPack Workbench and Utilities
Published by
Schneider Electric
Features
Functions
Custom IEC 61131-3 functions have been specifically designed by Schneider Electric for use with SCADAPack Smart RTUs.
These functions bring SCADA-specific operability to the IEC 61131-3 Workbench.
Backwards-Compatibility for Pre-Existing V3.x Programs
Workbench v.6 may be used to import existing SCADAPack program files created with Workbench v.3.
Programs, functions and FBs written in LD, ST and FBD may be edited and debugged after importing.
Program files written in Instruction List (IL), Sequential Function Chart (SFC) and Flow Chart (FC) languages may be imported and debugged, but not edited. Editing for IL, SFC and FC must be completed in Workbench v.3 before importing.
On-line Debugging and Monitoring
SCADAPack Workbench supports on-line debugging and monitoring of program logic.
While in the debug mode, code written in any of the graphic-based languages can be viewed in real-time, with indication of logic power flow and variable values.
Global and local variable values may also be viewed or forced from the dictionary and I/O wiring list views.
Concurrent C/C++ Code Execution
For additional programming power, an IEC 61131-3 application can execute in the SCADAPack Smart RTU concurrently with up to 32 independent C/C++ programs.
Process data generated in either application can be passed to the other.
This means, for example, that the results of complex mathematical algorithms, calculated using C/C++, can then be used by the IEC 61131-3 application to control the process.
SCADAPack Configurator
A companion application included with Workbench for controller-specific configurations and utilities including:
Communication port and protocol configuration
Controller firmware updating
File management operations
Real-time clock settings
Controller initialization
Functions
Backwards-Compatibility for Pre-Existing V3.x Programs
On-line Debugging and Monitoring
Concurrent C/C++ Code Execution
SCADAPack Configurator
A companion application included with Workbench for controller-specific configurations and utilities including:
Communication port and protocol configuration
Controller firmware updating
File management operations
Real-time clock settings
Controller initialization