ASi-5 Module with integrated IO-Link Master (BWU4067)
Simply integrating IO-Link into SE applications
Published by
Bihl+Wiedemann GmbH

ASi-5 Module with integrated IO-Link Master (BWU4067)
Published by
Bihl+Wiedemann GmbH
Features
Integrated OPC UA server
Thanks to the integrated OPC UA server in our gateways, process and diagnostic data of IO-Link devices can be transferred to the cloud in an easy and cost-efficient way.
One Ethernet connection for all ASi modules
One single Ethernet connection for all ASi modules linked to the ASi network required. The Ethernet connection is integrated in the ASi-5/ASi-3 Fieldbus Gateway from Bihl+Wiedemann
Fine-grained, flexible portfolio
The range of IO-Link masters contains 1-, 2-, 4- and 8-port versions
Even one single IO-Link device can therefore easily be connected at any location, distributed over the AS-Interface cable length of up to 200 meters
No "unused" IO-Link ports
One cable for standard and safety
Standard sensors and safety modules are all connected to one single 2-wire cable
Manufacturer-neutral linking
Manufacturer neutrality and interoperability in terms of:
sensors
higher-level controllers with their differing fieldbus interfaces
IO-Link devices from different manufacturers in the same network
Software tools for parameter setting
Parameter setting of the connected IO-Link sensors using B+W software suites
Online bus information makes it easy to commission ASi modules and IO-Link devices
Free choice of topology
Thanks to ASi, there are absolutely no restrictions on topology
Integrated OPC UA server
Thanks to the integrated OPC UA server in our gateways, process and diagnostic data of IO-Link devices can be transferred to the cloud in an easy and cost-efficient way.

One Ethernet connection for all ASi modules
One single Ethernet connection for all ASi modules linked to the ASi network required. The Ethernet connection is integrated in the ASi-5/ASi-3 Fieldbus Gateway from Bihl+Wiedemann
Fine-grained, flexible portfolio

One cable for standard and safety
Standard sensors and safety modules are all connected to one single 2-wire cable
Manufacturer-neutral linking
Manufacturer neutrality and interoperability in terms of:
Software tools for parameter setting

Free choice of topology
Thanks to ASi, there are absolutely no restrictions on topology