![](https://d2uars7xkdmztq.cloudfront.net/app_resources/58536/thumbs_112/img787226229919190845.png)
![](https://d2uars7xkdmztq.cloudfront.net/app_resources/58536/thumbs_112/img787226229919190845.png)
Stratus ztC Edge
Docs & Videos
AVEVA Representative discusses how Stratus ztC Edge Delivers Edge to Edge Functionality
Michal Postula, formerly at AVEVA, discusses how edge architectures "are going to be the dominant architectures for the digital transformation" and details how ztC Edge provides fault tolerance, robustness, and rugged high availability.
Stratus ztC Edge Comparison
The Edge is not a computing environment where clean rooms and IT help is abundantly available. While many companies are looking for ways to modernize automation and expand operations, most of the solutions that get considered such as desktops and standalone servers and Industrial PCs don't offer the complete list of benefits required for today's Edge deployments. Stratus ztC Edge is the only purpose-built Edge solution enabling simple and always available virtualization for critical operations
Stratus ztC Edge and FacilityConneX Case Study
When Tom Schiller from FacilityConnex was investigating how best to run their new analytics software to work with the data collected by onsite historians he turned to the new ztC Edge from Stratus because of the simplicity and reliability that it brought to the Edge.