Worldwide Buildings Energy Consumption - Free edition

The data refers to 5 Schneider Electric buildings located worldwide and contains both metadata and timeseries
Published by Schneider Electric

Overview

Worldwide Buildings Energy Consumption - Free edition
The data refers to the energy consumption of 5 Schneider Electric buildings located worldwide, gathered over a 1-year period of time. It contains both metadata (building location, surface, occupancy as well as meters connected) and timeseries.

Each building can hold several main meters, depending on the measured WAGES (Water, Air, Gas, Electric, Steam), for an observation period ranging from one, to several years. The meters can be of two types: smart meter with near real time readings, and automatic meter with monthly readings.

The data originates from Schneider Electric's program to optimize energy consumption of SE Facilities.

Worldwide Buildings Energy Consumption - Free edition

Benefits

Large database of energy consumption in buildings
This large database enables data scientists to execute several building analysis, such as, building performances, bench-marking, buildings clustering, and building energy modelling.