ExtremeManagement
Published by
Extreme Networks
Features
Complete Integration
Intelligence, automation, and integration to optimize the efficiency of network operations.
Integrated wired/wireless management
-
Provides consistent management of both the wired and wireless network from a single interface. Scripting based automation reduces IT administration.
Dashboard and reports
-
Provides a graphical user interface for network data collection and reporting of network analytics. Impact analysis dashboard delivers deep insight and simplicity.
Open Application Programmatic Interface (API)
-
Provides an open and secure two-way interface into Management Center for third-party application integration and control of software defined networking (SDN) implementations.
Network Inventory Management
-
Advanced network configuration and change management for the wired and wireless infrastructure.
Historical data collection and trend analysis
-
Provides the ability to take flow-based data to understand how the network is being used up to layer 4. With the addition of Purview this extends the detailed analytics to the application layer (layer 7) for detailed application visibility across the entire network.
Policy-based network
-
Allows for the centralized creation of policies that follow users and devices across the network. These are not tied to the physical network and can change based on user, device, TOD, location, and connection type.
Identity and access control
-
Provides visibility and control down to the user and device level.
Intelligent alarm management
-
Alarm and event intelligence that alert IT when issues occur within the network are automatically cleared when the problem no longer exists and allows thresholds to be set so that warnings are sent prior to an actual failure.
Troubleshooting
-
Eliminates the guesswork and makes troubleshooting user issues easy. Just enter the username and discover where the user is located, where they are connected on the network, the type of device they are using, and much more.
Third-party network integration
-
Manage third-party devices to provide a complete picture of the entire infrastructure in a heterogeneous network environment.
Complete Integration
Intelligence, automation, and integration to optimize the efficiency of network operations.
Integrated wired/wireless management
- Provides consistent management of both the wired and wireless network from a single interface. Scripting based automation reduces IT administration.
Dashboard and reports
- Provides a graphical user interface for network data collection and reporting of network analytics. Impact analysis dashboard delivers deep insight and simplicity.
Open Application Programmatic Interface (API)
- Provides an open and secure two-way interface into Management Center for third-party application integration and control of software defined networking (SDN) implementations.
Network Inventory Management
- Advanced network configuration and change management for the wired and wireless infrastructure.
Historical data collection and trend analysis
- Provides the ability to take flow-based data to understand how the network is being used up to layer 4. With the addition of Purview this extends the detailed analytics to the application layer (layer 7) for detailed application visibility across the entire network.
Policy-based network
- Allows for the centralized creation of policies that follow users and devices across the network. These are not tied to the physical network and can change based on user, device, TOD, location, and connection type.
Identity and access control
- Provides visibility and control down to the user and device level.
Intelligent alarm management
- Alarm and event intelligence that alert IT when issues occur within the network are automatically cleared when the problem no longer exists and allows thresholds to be set so that warnings are sent prior to an actual failure.
Troubleshooting
- Eliminates the guesswork and makes troubleshooting user issues easy. Just enter the username and discover where the user is located, where they are connected on the network, the type of device they are using, and much more.
Third-party network integration
- Manage third-party devices to provide a complete picture of the entire infrastructure in a heterogeneous network environment.