SE.AppFunctional library for EcoStruxure™ Automation Expert

Application functional library
Published by Schneider Electric

Overview

EcoStruxure™ Automation Expert functional templates (Analog, Binary, Utilities)

EcoStruxure™ Automation Expert application library package is a set of reusable objects using IEC 61499 control application and SE.AppFunctional library that included functional assets, will be removed in the EcoStruxure™ Automation Expert v22.2 as it has been replaced by the SE.AppBase and SE.AppCommonProcess that provides adapters. Schneider Electric strongly recommends users to update their application by using SE.AppBase / SE.AppCommonProcess library.


This library is a template collection of Composite Automation Templates (Analog, Binary, Utilities) that have been tested and validated by Schneider Electric to help in quicker deployment with less challenges during commissioning of the EcoStruxure™ Automation Expert, providing:

  • EcoStruxure™ Automation Expert HMI object
  • Alarm management based on ISA 18.2
  • Important Note:


    The .zip file includes the fblib of the SE.AppBase library versions as listed below:

  • v21.1.0.13 - Compatible with EcoStruxure™ Automation Expert v21.1
  • v21.1.0.10 - Compatible with EcoStruxure™ Automation Expert v21.1
  • v20.2.0.27 - Compatible with EcoStruxure™ Automation Expert v20.2 and v21.1
  • SE.AppFunctional library for EcoStruxure™ Automation Expert

    Benefits

    Simplify engineering & deployment; reducing cost

    • Ready-to-use automation objects to reduce engineering lead time.
    • Tested and validated Libraries help in quick deployment with less challenges during commissioning of systems.

    Enable Operation & Maintenance Excellence

    • Build domain know how into Libraries to improve operational performance.
    • Manage Energy Measurement & performance trends.
    • Provide Asset Performance information and manage maintenance data.
    Unauthorised background image

    Your product is just steps away!

    Register for FREE to buy, get downloads and access free trials.

    Get Resources and Start FREE Trials

    Easy Product Activation with Your Account

    Products Saved to Personal Digital Library