SE.AppConveying library for EcoStruxure™ Automation Expert
Conveying library
Published by
Schneider Electric

SE.AppConveying library for EcoStruxure™ Automation Expert
Published by
Schneider Electric
Free
Features
Simplify engineering & deployment
Ready-to-use automation objects to reduce engineering lead time
Tested and validated Libraries help in quick deployment with less challenges during commissioning of systems
Supported functions
The SE.AppConveying provides elementary control and visualization functions for your automation system, it includes:
Elementary Modules
Conveyor Base (This conveyor moves in two directions with speed and has a zone sensor for the presence of goods)
Pusher (Pushes the goods from one conveyor system to another)
Side Input (Manages side input to main line)
Transfer Table (Lifts the good)
Turntable (Moves the good in forward and reverse direction)
Logic Solver (TransLogicSolver, TurntableLogicSolver)
EcoStruxure™ Automation Expert HMI Objects
The SE.AppConveying provides symbols and faceplates for each CAT ready to be used in the EcoStruxure™ Automation Expert HMI.
Simplify engineering & deployment

Supported functions
The SE.AppConveying provides elementary control and visualization functions for your automation system, it includes:
Elementary Modules
EcoStruxure™ Automation Expert HMI Objects
The SE.AppConveying provides symbols and faceplates for each CAT ready to be used in the EcoStruxure™ Automation Expert HMI.