SE.AppConveying library for EcoStruxure™ Automation Expert

Conveying library
Published by Schneider Electric

Overview

EcoStruxure™ Automation Expert conveying template (Conveyor, Pusher, Table)

EcoStruxure™ Automation Expert application library package is a set of reusable objects using IEC 61499 control application and SE.AppConveying is used to monitor and manage a conveyor.


This library is a template collection of Composite Automation Templates (Conveyor, Pusher, Table) that have been tested and validated by Schneider Electric to help in quicker deployment with less challenges during commissioning of the EcoStruxure™ Automation Expert, providing:

  • Visualization based on Situational Awareness
  • EcoStruxure™ Automation Expert HMI object
  • Alarm management based on ISA 18.2
  • Easy Customization to customer’s needs/habits
  • Important Note:


    The .zip file includes the fblib of the SE.AppBase library versions as listed below:

  • v21.1.0.8 - Compatible with EcoStruxure™ Automation Expert v21.1
  • v21.1.0.5 - Compatible with EcoStruxure™ Automation Expert v21.1
  • SE.AppConveying library for EcoStruxure™ Automation Expert

    Benefits

    Simplify engineering & deployment; reducing cost

    • Ready-to-use automation objects to reduce engineering lead time.
    • Tested and validated Libraries help in quick deployment with less challenges during commissioning of systems.

    Enable operation & maintenance excellence

    • Build domain know how into Libraries to improve operational performance.
    • Manage Energy Measurement & performance trends.
    • Provide Asset Performance information and manage maintenance data.

    Customization

    • All the blocks are available for your project. Helping you build the objects which may be unique to your system.
    • An issue with one block can be customized without invalidating the other blocks in the library.

    Reusability

    • The same components are used repeatedly to achieve the same task. They are proven and understood.
    Unauthorised background image

    Your product is just steps away!

    Register for FREE to buy, get downloads and access free trials.

    Get Resources and Start FREE Trials

    Easy Product Activation with Your Account

    Products Saved to Personal Digital Library