NEST i4.0 for EcoStruxure™ Plant and Machine
Vibration monitoring and diagnosis for rotating machines
Published by
ACOEM

NEST i4.0 for EcoStruxure™ Plant and Machine
Published by
ACOEM
Features
Easy machinery setup
It’s enough to drag & drop machinery components with seamless graphic tools to create machines. All the necessary measurement parameters are automatically assigned taking into consideration the type and power of the machine and the rotation speed(s).
Smart diagnosis
With more than 50 years of expertise in predictive maintenance technology, ACOEM has integrated powerful indicators in the NEST i4.0 system. Parameters like the Bearing Defect Factor, the Shock Finder Index or HarmoniX Index provide meaningful machinery health status in an easy-to-understand Health Matrix.
Guided analysis
Lists of machines filtered according to their health status together with smart indexes help the vibration analyst to focus his attention on machines which really need to be looked at in detail.
Vibration analysts can save up to 30% additional time in periodical analysis.
Automatic reporting
Customizable reports can be automatically generated on one or multiple machines at a time. They include the synthesis of the assets health, a powerful ACCUREX Diagnostic Matrix showing green-yellow-red indicators for 9 typical faults, the detailed diagnostics and maintenance recommendations, as well as all monitoring indicators values and alarms.
EcoStruxure™ connectivity
NEST i4.0 is an open data platform with OPC UA and CSV connectors useful to publish actionable machinery health indicators together with ISO standard thresholds, diagnosis and recommendations to EcoStruxure™ applications
EAGLE wireless IIoT
The EAGLE wireless vibration sensors are extremely easy to install to ensure the monitoring of e.g. pumps, fans or gearboxes. Every day and/or every hour, the measured temperature and vibration signals are automatically sent to the NEST i4.0 software for enhanced ACCUREX automatic diagnosis processing and expert analysis if required. The EAGLE wireless sensors can also publish overall indicators directly to EcoStruxure applications through a Modbus TCP connection.
MVx online IIoT
The MVx online system embeds outstanding features to monitor the most critical machines operating at variable conditions (different rotation speeds, loads, torques, pressures, etc.). The MVx system continuously acquires vibration and/or other signals to provide proven alerts in real-time. Both smart indicators and alerts can be published to EcoStruxure™ applications through a Modbus TCP connection. Moreover, the measured data are automatically sent to the NEST i4.0 software for expert analysis and diagnosis.
Easy machinery setup
It’s enough to drag & drop machinery components with seamless graphic tools to create machines. All the necessary measurement parameters are automatically assigned taking into consideration the type and power of the machine and the rotation speed(s).

Smart diagnosis
With more than 50 years of expertise in predictive maintenance technology, ACOEM has integrated powerful indicators in the NEST i4.0 system. Parameters like the Bearing Defect Factor, the Shock Finder Index or HarmoniX Index provide meaningful machinery health status in an easy-to-understand Health Matrix.

Guided analysis
Lists of machines filtered according to their health status together with smart indexes help the vibration analyst to focus his attention on machines which really need to be looked at in detail.
Vibration analysts can save up to 30% additional time in periodical analysis.

Automatic reporting
Customizable reports can be automatically generated on one or multiple machines at a time. They include the synthesis of the assets health, a powerful ACCUREX Diagnostic Matrix showing green-yellow-red indicators for 9 typical faults, the detailed diagnostics and maintenance recommendations, as well as all monitoring indicators values and alarms.

EcoStruxure™ connectivity
NEST i4.0 is an open data platform with OPC UA and CSV connectors useful to publish actionable machinery health indicators together with ISO standard thresholds, diagnosis and recommendations to EcoStruxure™ applications

EAGLE wireless IIoT
The EAGLE wireless vibration sensors are extremely easy to install to ensure the monitoring of e.g. pumps, fans or gearboxes. Every day and/or every hour, the measured temperature and vibration signals are automatically sent to the NEST i4.0 software for enhanced ACCUREX automatic diagnosis processing and expert analysis if required. The EAGLE wireless sensors can also publish overall indicators directly to EcoStruxure applications through a Modbus TCP connection.

MVx online IIoT
The MVx online system embeds outstanding features to monitor the most critical machines operating at variable conditions (different rotation speeds, loads, torques, pressures, etc.). The MVx system continuously acquires vibration and/or other signals to provide proven alerts in real-time. Both smart indicators and alerts can be published to EcoStruxure™ applications through a Modbus TCP connection. Moreover, the measured data are automatically sent to the NEST i4.0 software for expert analysis and diagnosis.