TRIO™ Q Data Radio Firmware

TRIO™ Q Data Radio Firmware
Docs & Videos
Trio Q Data Radio – IP Routing benefits & configuration
This video will present the benefits of IP Routing in the Trio Q licensed data radio, as well as show the basic configuration required.
How to create a Point to Point network with the Trio Q Radio
The trainee will be able to create a point to point Radio network using two Trio Q data radios for exchanging data over the air with a licensed frequency.
Trio Q Series licensed radio – Demonstration using the wizard
This video will present the process of setting up a pair of Trio QR450 licensed radios for demonstration or test purposes using the built-in Wizard configuration tool.
Trio Q VHF data radio – Advantages and new features
In this video we share the new features of the Trio Q VHF licensed data radios and will demonstrate the advantages of using the VHF frequency band.
Global firmware updating - For the Trio Q data radio
his video will discuss the benefits of the Global Firmware Update tool that is available for the Trio Q licensed data radio, and then provide a quick demonstration.
Trio Q series licensed radio – Dynamic speed mode
This video will discuss the benefits of the Dynamic radio data rate feature in the Trio Q Series licensed radio, and then briefly show how the radios are configured to make use of this mode.
Trio Q data radio compatibility with E series
In this video the viewer will learn how to configure the Trio Q data radio to operate in e series compatibility mode within a Trio E series radio network.
Trio Q Data Radio Alarms and Events
In this video the viewer will discover how to view alarms and events in the Trio Q data radio, and learn how to configure custom alarm settings.
How to use the text user interface with a Trio Q data radio
The trainee will be able to establish communications with the Trio Q Data Radio using the Text User interface for low bandwidth communications. The text user interface (TUI) provides an alternative to the HTML web user interface for configuration and diagnostics. The TUI can be accessed directly from the serial port of the Q data radio or via a telnet or SSH session. The TUI is enabled on COM 1 by default, while Telnet is also enabled by default, however, this requires an Ethernet connection.
Trio Q data radio – Multi user access
In this video by Joel Weder, the viewer will learn how to implement and use the multi-user access features of the Trio Q Data Radio.
Quadrature Amplitude Modulation (QAM) in Trio Q Radios
Explore the features and benefits of Quadrature Amplitude Modulation in the Trio Q Data Radio, along with related tools including Trio's innovative implementation of Forward Error Correction and Dynamic Speed Selection.
Trio Q - Token grant channel management
Join Telemetry Solutions Specialist Joel Weder in a tour of the Token Grant Channel Management feature found in the Trio Q Series of innovative remote data radios.
Trio Q series - Radio access control
Join SCADA and Telemetry Specialist Joel Weder for an in-depth look at the Radio Access Control feature built-in to our Trio Q-series of security-enhanced data radios.