SoundEar 3-300
Features
SoundEar3 Software: Map your Noise Levels
Use the SoundEar3 Software to stay on top of your noise levels and make sure you are always up to date with how your noise situation looks.
You can use the software to provide documentation on noise levels and to perform noise mapping for your company.
Monitor noise levels live for one or more locations.
Compare and analyze noise levels across time and locations.
Automate the process of staying on track: Use automated noise reports.
Where to use SoundEar 3-300
The SoundEar3-300 can be used when you need to control noise at a hospital. It is most often used in,
Patient rooms
Recovery rooms
Operation theatres
Intensive Care Units
Neonatal Care
How to use SoundEar 3-300
There are different ways to use the SoundEar3 software, depending on the way you want to use your SoundEar3 device(s):
Manual method
You have one or a few SoundEar3 devices, and do not mind a few manual touches to the process of getting your data.
In this case you will be collecting your noise measurements via a USB key, that you insert into the device to download your measurements.
Next, you can view your measurements in the software, using the Import from USB function.
Refer video in Resources section on how to download and view noise measurements using the manual method.
Automated method
You have a number of SoundEar3 devices, and you want the process of collecting data to be automatic.
In this case you set up your system to receive measurements via your preferred method: Wireless (via radio signal), Wireless (via Wi-Fi & Cloud Service), Cabled (via LAN).
Your noise measurements will automatically be collected and displayed in the SoundEar Software, as long as the software is running.
One example of using the automated noise reports:
One report is sent once a week with a summarized overview (for administrators, top level management, etc.)
One report is sent once a day with a more detailed overview (for mid-level management, controllers, etc.)
One report is sent several times a day, e.g. one for each shift (for first level management, employees, etc.)
SoundEar3 Software: Map your Noise Levels
Use the SoundEar3 Software to stay on top of your noise levels and make sure you are always up to date with how your noise situation looks.
You can use the software to provide documentation on noise levels and to perform noise mapping for your company.
Where to use SoundEar 3-300
The SoundEar3-300 can be used when you need to control noise at a hospital. It is most often used in,
How to use SoundEar 3-300
There are different ways to use the SoundEar3 software, depending on the way you want to use your SoundEar3 device(s):
Manual method
You have one or a few SoundEar3 devices, and do not mind a few manual touches to the process of getting your data.
Refer video in Resources section on how to download and view noise measurements using the manual method.
Automated method
You have a number of SoundEar3 devices, and you want the process of collecting data to be automatic.
One example of using the automated noise reports: