EcoStruxure™ Control Expert - HVAC Library

Heating, Ventilation and Air Conditioning Solutions EFB Library
Published by Schneider Electric

Overview

Function blocks of the Modicon Libraries - HVAC library

EcoStruxure™ Control Expert - HVAC Library provides solution for Air Conditioning with

  • Accurate Temperature and Humidity Control
  • Maintain comfort conditioning and air quality
  • Filtrate the supplied air to remove the particles and microorganisms
  • Reduce airborne infections
  • Not a source of bacterial and fungal growth
  • Control Oduor

  • Library implements the Air Conditioning solution as EFBs (elementary function blocks) in Control Expert


    The EFBs provide ready to use solutions, Easy setup and modification


    Compatible with

  • EcoStruxure™ Control Expert V15 and above
  • NOTE: Click on the Download button to download the software package. However, user need to purchase a License to be able to install the Library in EcoStruxure™ Control Expert

    EcoStruxure™ Control Expert - HVAC Library

    Benefits

    Ready to use 11 Function Blocks

    6 basic function blocks (Basic Group)

  • The basic function blocks implement low level functions for basic air conditioning solutions

  • 5 complex function blocks (Complex Group)

  • The complex function blocks implement the more complex functions found in controllers which are frequently used in air conditioning systems. They are built using the basic function blocks
  • Solution that meets Standards

    This Library provide Solutions which meets standards

    Application Control need winter/summer setpoint compensation as per DIN 1946 pert 2


    Operation with Anti–Windup–Reset (AWR)

    Unauthorised background image

    Your product is just steps away!

    Register for FREE to buy, get downloads and access free trials.

    Get Resources and Start FREE Trials

    Easy Product Activation with Your Account

    Products Saved to Personal Digital Library