HMI Screen Templates for EcoStruxure™ Machine SCADA Expert

Project screen templates suitable for EcoStruxure™ Machine SCADA Expert
Published by Schneider Electric

Features

  • Contents of file

Contents of file

  • Navigation layout
  • Alarm
  • Trend
  • Energy management
  • Bar graph
  • Recipes
  • Scheduler
  • Database
  • PackML etc.
  • Note: the minimum software version required for each of the templates is indicated in the name of the file (example: EcoStruxureMSE_8.1.5_* projects can be opened with 8.1 SP5 software version or later).