Plant iT
Published by
ProLeiT GmbH
Overview
Cutting-edge process control technology. Including MES.
Plant iT is an integrated and modular software platform, consisting of base systems, modules and add-ons which can be combined flexibly. The base systems as well as the modules and add-ons, are seamlessly integrated, with a central user interface across the system.
All basic Plant iT systems have a central engineering environment with a shared database and an integrated parameterisation interface. All the modules can be optionally combined with the basic systems, ensuring that the appropriate Plant iT system can be implemented to form an industry 4.0 smart factory.
Plant iT is an object-oriented and PLC-based process control system with integrated manufacturing execution system (MES) functionality developed by ProLeiT GmbH. It can be used in combination with PLCs from various manufacturers and is available in five language versions. Thats why automation solutions based on Plant iT and brewmaxx are used in more than 110 countries around the globe.
Cutting-edge process control technology. Including MES.
Plant iT is an integrated and modular software platform, consisting of base systems, modules and add-ons which can be combined flexibly. The base systems as well as the modules and add-ons, are seamlessly integrated, with a central user interface across the system.
All basic Plant iT systems have a central engineering environment with a shared database and an integrated parameterisation interface. All the modules can be optionally combined with the basic systems, ensuring that the appropriate Plant iT system can be implemented to form an industry 4.0 smart factory.
Plant iT is an object-oriented and PLC-based process control system with integrated manufacturing execution system (MES) functionality developed by ProLeiT GmbH. It can be used in combination with PLCs from various manufacturers and is available in five language versions. Thats why automation solutions based on Plant iT and brewmaxx are used in more than 110 countries around the globe.
All basic Plant iT systems have a central engineering environment with a shared database and an integrated parameterisation interface. All the modules can be optionally combined with the basic systems, ensuring that the appropriate Plant iT system can be implemented to form an industry 4.0 smart factory.
Plant iT is an object-oriented and PLC-based process control system with integrated manufacturing execution system (MES) functionality developed by ProLeiT GmbH. It can be used in combination with PLCs from various manufacturers and is available in five language versions. Thats why automation solutions based on Plant iT and brewmaxx are used in more than 110 countries around the globe.