ADA
Overview
Cloud-based service for providing optimized performance for HVAC systems
ADA is a powerful optimization software that will optimize the control settings of your HVAC system. ADA deploys advanced algorithms and Machine Learning to find the optimal settings in order to reach a desired air quality at the lowest possible energy consumption.
ADA is an add-on service that lowers the energy consumption of HVAC systems without compromising the air quality. The service is integrated with existing equipment and via sensors, ADA measures indoor and outdoor air quality and how it changes.
Based on the customers requirement on indoor air quality and comfort, optimal set points are calculated to cope with the current load and adapts to the change in the load. Automatically and continuously in real time ADA feeds the original control with the most economical solution for achieving specified air quality levels, no matter what the existing conditions are.
Cloud-based service for providing optimized performance for HVAC systems
ADA is a powerful optimization software that will optimize the control settings of your HVAC system. ADA deploys advanced algorithms and Machine Learning to find the optimal settings in order to reach a desired air quality at the lowest possible energy consumption.
ADA is an add-on service that lowers the energy consumption of HVAC systems without compromising the air quality. The service is integrated with existing equipment and via sensors, ADA measures indoor and outdoor air quality and how it changes.
Based on the customers requirement on indoor air quality and comfort, optimal set points are calculated to cope with the current load and adapts to the change in the load. Automatically and continuously in real time ADA feeds the original control with the most economical solution for achieving specified air quality levels, no matter what the existing conditions are.