X-Force Alarm Information Management System
All in one alarm management solution
Published by
SSM InfoTech Solutions Pvt. Ltd.

X-Force Alarm Information Management System
Published by
SSM InfoTech Solutions Pvt. Ltd.
Features
Easy to integrate
Integrate with any make of DCS/PLC/SCADA. Supports all types of communication protocols such as ethernet, serial, OPC-DA, OPC-AE, ODBC, File based or any proprietary communication
Alarm suppression and shelving
Hide or temporarily disable nuisance alarms that are irrelevant or distracting to the operator, allowing them to keep focused on alarms that need attention.
Alarm discrepancy analysis
During the change in value of any master set point, the report on the deviations against compliance occurs automatically.
Track operator actions
X-Force AIMS allows user to track operator actions to improve operator efficiency. Track every set point change or OA changes during the shift.
Most critical alarm handling module
Separate out the nuisance alarm from the most critical ones that gives a wide overview on handling critical alarms at a priority.
Reporting & analytics
- Identify and eliminate chattering and predictable alarms.
- Benchmark alarm system performance against industry standards.
- More than 50 analysis reports for Process and Non-Process plant activity to get insights on plant condition.
- Get fully customized reports as per the user requirements.
- Comes with Reports Module: 15 types of reports as per EEMUA guidelines.
Notifications
Email module & SMS (Text) notification module along with Emergency Hooter and PA system Connectivity Module
Dynamic alarming
Ensure system performance remains robust even during state transitions and process upsets. X-Force KPI Reporting tool identifies precisely where advance alarming techniques will yield the maximum number of investment.
KPI dashboards
KPI Dashboards for overall plant process status along with daily, weekly and monthly analytics dashboard for plant or site. Faster and easy access to plant data for higher management like for HOD, VC, etc.
Easy to integrate
Integrate with any make of DCS/PLC/SCADA. Supports all types of communication protocols such as ethernet, serial, OPC-DA, OPC-AE, ODBC, File based or any proprietary communication

Alarm suppression and shelving
Hide or temporarily disable nuisance alarms that are irrelevant or distracting to the operator, allowing them to keep focused on alarms that need attention.
Alarm discrepancy analysis
During the change in value of any master set point, the report on the deviations against compliance occurs automatically.
Track operator actions
X-Force AIMS allows user to track operator actions to improve operator efficiency. Track every set point change or OA changes during the shift.
Most critical alarm handling module
Separate out the nuisance alarm from the most critical ones that gives a wide overview on handling critical alarms at a priority.
Reporting & analytics
- - Identify and eliminate chattering and predictable alarms.
- - Benchmark alarm system performance against industry standards.
- - More than 50 analysis reports for Process and Non-Process plant activity to get insights on plant condition.
- - Get fully customized reports as per the user requirements.
- - Comes with Reports Module: 15 types of reports as per EEMUA guidelines.
Notifications
Email module & SMS (Text) notification module along with Emergency Hooter and PA system Connectivity Module

Dynamic alarming
Ensure system performance remains robust even during state transitions and process upsets. X-Force KPI Reporting tool identifies precisely where advance alarming techniques will yield the maximum number of investment.
KPI dashboards
KPI Dashboards for overall plant process status along with daily, weekly and monthly analytics dashboard for plant or site. Faster and easy access to plant data for higher management like for HOD, VC, etc.