X-Force Alarm Information Management System

X-Force Alarm Information Management System
Overview
Industrial Alarm Information Management System for process safety
Industries generally lack advanced reporting facilities and centralized monitoring for various Alarm Information Systems. DCS/PLC/SCADA sources have limited device configuration and therefore it causes alarm flood, standing alarms, nuisance alarm. This in turn costs time, resources, and money and non-complaint with EEMUA 191, ANSI/ISA-18.2-2009, IEC 62682, EPRI global standards.
X-Force Alarm Information Management System (AIMS) consists of updated modules to integrate all alarm-related data from the vendor agnostics system into a single centralized station, so that operators can identify the actual alarm generation and determine the root cause to respond promptly and prevent any economic/physical loss.
X-Force AIMS stores data on its Local Server / Enterprise Server and provides access to users of its powerful analytics on received Alarms. This helps the plant users and operators to detect the exact origin of alarms from various areas and take the rationalized decision.
Industrial Alarm Information Management System for process safety
Industries generally lack advanced reporting facilities and centralized monitoring for various Alarm Information Systems. DCS/PLC/SCADA sources have limited device configuration and therefore it causes alarm flood, standing alarms, nuisance alarm. This in turn costs time, resources, and money and non-complaint with EEMUA 191, ANSI/ISA-18.2-2009, IEC 62682, EPRI global standards.
X-Force Alarm Information Management System (AIMS) consists of updated modules to integrate all alarm-related data from the vendor agnostics system into a single centralized station, so that operators can identify the actual alarm generation and determine the root cause to respond promptly and prevent any economic/physical loss. X-Force AIMS stores data on its Local Server / Enterprise Server and provides access to users of its powerful analytics on received Alarms. This helps the plant users and operators to detect the exact origin of alarms from various areas and take the rationalized decision.