EcoStruxure™ Operator Terminal Expert Runtime

Touchscreen configuration software with the latest UI design and gestures
Published by Schneider Electric

Overview

Human Machine Interface software to create and edit application Harmony HMIs and iPCs screens

EcoStruxure™ Operator Terminal Expert is an innovative Human Machine Interface software which provides new navigation options and allows you to create personalised user guidance and data handling.It helps operators to maximize efficiency through modern functionalities and user-friendly features


This installer is the RunTime installer, to be used in case you need to have EcoStruxure™ Operator Terminal Expert projects running on Harmony industrial PCs or 3rd party Windows Operating System machines.


Available version for download is the version 3.2 SP1.

EcoStruxure™ Operator Terminal Expert Runtime

Benefits

Develop the most intuitive industrial HMI

Supports smartphone like gestures like pinch zoom, scroll and swipe.

Reduce the total cost of ownership

Cross-Platform HMI technology (Windows and Linux).

Efficient design

Automatic navigation menus - Pages larger than the screen size