TVIEW+™ for Trio™ Data Radios
TVIEW+™ for Trio™ Data Radios
Docs & Videos
Quadrature Amplitude Modulation (QAM) in Trio Q Radios
Explore the features and benefits of Quadrature Amplitude Modulation in the Trio Q Data Radio, along with related tools including Trio's innovative implementation of Forward Error Correction and Dynamic Speed Selection.
Trio Q - Token Grant Channel Management
Join Telemetry Solutions Specialist Joel Weder in a tour of the Token Grant Channel Management feature found in the Trio Q Series of innovative remote data radios.
Trio Q Data Radio – IP Routing Benefits & Configuration
This video presents the benefits of IP Routing in the Trio Q licensed data radio, as well as show the basic configuration required.
Trio Ethernet Radios – Internal Diagnostic Features
This video discusses the diagnostic capabilities that are available built into the Trio Q Series licensed data radio and the J Series license-free radio, and then will provide a brief demonstration of each.
How to Create a Point to Point Network with the Trio Q Radio
After viewing this video, the trainee will be able to create a point to point Radio network using two Trio Q data radios for exchanging data over the air with a licensed frequency.
Trio J Series Configuration with WUI and Diagnostic with TView Video Tutorial
In this video, learn how to configure the Trio Q Series data radio with the web-based user interface and view a Diagnostics tutorial in TVIEW+
Trio Q Series Licensed Radio – Demonstration Using the Wizard
This video presents the process of setting up a pair of Trio QR450 licensed radios for demonstration or test purposes using the built-in Wizard configuration tool.
Trio Q VHF Data Radio – Advantages and New Features
In this video we share the new features of the Trio Q VHF licensed data radios and will demonstrate the advantages of using the VHF frequency band.
Global Firmware Updating - For the Trio Q Data Radio
This video discusses the benefits of the Global Firmware Update tool that is available for the Trio Q licensed data radio, and then provide a quick demonstration.
Trio Q Data Radio – Multi-User Access
In this video by Joel Weder, the viewer will learn how to implement and use the multi-user access features of the Trio Q Data Radio.
Trio Q Series Licensed Radio – Dynamic Speed Mode
This video discusses the benefits of the Dynamic radio data rate feature in the Trio Q Series licensed radio, and then briefly show how the radios are configured to make use of this mode.
Trio Q Data Radio Compatibility with E Series
In this video the viewer will learn how to configure the Trio Q data radio to operate in e series compatibility mode within a Trio E series radio network.
Trio Q Data Radio Alarms and Events
In this video the viewer will discover how to view alarms and events in the Trio Q data radio, and learn how to configure custom alarm settings.
How to use the Text User Interface with a Trio Q Data Radio
After viewing this video, the trainee will be able to establish communications with the Trio Q Data Radio using the Text User interface for low bandwidth communications. The text user interface (TUI) provides an alternative to the HTML web user interface for configuration and diagnostics.
Trio Ethernet Radios – Modbus Gateway and Serial Server
Watch this video to learn how to configure the Modbus Gateway and Serial Device Server features of the Trio Ethernet Data Radio.
How to Setup a Point to Point Network with the Trio J Data Radio
After viewing this video, the trainee will be able to create a point to point radio network using two Trio J data radios for exchanging data over the air with a license free frequency.
How to use the Spectrum Analyzer & Channel Lockout Facility with the Trio J Data Radio
The Spectrum Analyzer is a facility that allows user to observe interfering signals in the ISM band. In Access Point radios, channels that suffer from high levels of interference can be blocked out of the hopping pattern. The spectrum analyzer can only be accessed via the Text User Interface (TUI). The spectrum analyzer and channel lock out facility is not available on Brazilian-compliant model types.
Trio K Series License-Free Radio - Wizard Demo
This video discusses how to quickly set up a small Trio K Series license-free radio system to perform a test or a demonstration, using the Wizard tool in the TView+ K Series programming software.
Trio M Series Licensed Radio - Basic Configuration
This video demonstrates how easy it is to do basic configuration of the Trio M Series serial licensed data radio and to perform diagnostic testing.