EcoStruxure™ Geo SCADA Expert – Sparkplug B Sample Driver

Simple Driver Development Kit Sample Driver
Published by Schneider Electric

Features

  • Development Kit
  • Automation

Development Kit

The driver is offered as source code which you can build with Visual Studio. It includes the two parts of the driver and an installer, enabling you to build a package to deploy to Geo SCADA Expert servers.

The source code is available for you to freely use, modify and extend to suit your requirements or that of your clients. It is not the most optimized, efficient or elegant code, and the functionality is not assured in the way the core product is, but we hope that its simplicity will encourage engagement with the Geo SCADA driver development process and explore the new ideas presented for Sparkplug B implementation with Geo SCADA.

The functionality in the driver includes basic data processing, and the feature which we hope will stimulate innovation and conversation is the built-in automatic configuration facility. This integrates well with the Geo SCADA template and instance features.

Automation

Integration with the Geo SCADA Expert configuration features is included:
  • Automatically create devices and points
  • Automatically set properties of points
  • Link device types to templates
  • Automatically find and instance templates containing displays and trends
  • Automation