VOSySmonitor

Low Latency Certified virtualization solution for Mixed-Criticality Systems

Features

  • Mixed critical virtualization
  • Security
  • Efficient virtualization

Mixed critical virtualization

Possibility to run operating systems with different levels of criticality (e.g., Linux and a RTOS) on the same hardware.
Mixed critical virtualization

Security

VOSySmonitor can host a Trusted Execution Environment (TEE) together with Linux and FreeRTOS. Such TEE is then able to enhance the security of the system.
Security

Efficient virtualization

VOSySmonitor is a low level partitioner that creates two execution environments to host different operating systems. No overhead is added to the system, as guests execute directly on the hardware.