PLC-Easy

Library for M340, M580 Epacs and Wonderware
Published by PLC-Easy
Starts at $20

Editions & Pricing

All Plans Include
  • Control and Digital Modules can't be purchased in the same shopping card.
  • If you are buying a Control Module, please return to the product page to create another shopping card and purchase a Digital Module.
  • Note: you can't create two shopping cards at once.
Control module
  • $200.00 / module one time
    For 1-1000 Modules
  • $150.00 / module one time
    For 1001-2000 Modules
  • $100.00 / module one time
    For 2001 Modules And Above
  • Ideal For
    • End user
    Included
    • 1 User
    • The license is bound to a single EPAC (or redundant pair) and can only be used for that device/redundant pair
    • The control modules/ software blocks allows you to build a controls application.
    Digital Module
  • $20.00 / module one time
    For 1-1000 Modules
  • $15.00 / module one time
    For 1001-2000 Modules
  • $10.00 / module one time
    For 2001 Modules And Above
  • Ideal For
    • End user
    Included
    • 1 User
    • The license is bound to a single EPAC (or redundant pair) and can only be used for that device/redundant pair
    • The digital blocks allows you to integrate any on/off signal into the application and make use of the inbuilt messaging system (to create an alarm message, warning message, status message, root cause message etc.)
    Unauthorised background image

    Your product is just steps away!

    Register for FREE to buy, get downloads and access free trials.

    Get Resources and Start FREE Trials

    Easy Product Activation with Your Account

    Products Saved to Personal Digital Library