Caneco Implantation
Published by
ALPI
Features
Implantation of electrical equipment
Caneco Implantation main features include the implantation of electrical equipment in 2D/3D as well as the optimization of cable routing.
Caneco Implantation integrates a Low Voltage (LV) and Extra Low Voltage (ELV) object library that comprises distribution boards and cabinets, lighting features, specific and general purpose sockets outlets, cable trays, etc.
Caneco Implantation enables you to customize electrical equipment in the library and to add also symbols created in AutoCAD®.
Caneco Implantation allows you to import lighting features installed in Dialux® after the illumination calculations have been completed.
Sizing and calculations
Caneco Implantation exports the created circuits to Caneco BT, which in turn calculates the cross-section of cables and also the protective devices.
The results are then re-imported into Caneco Implantation.
Caneco Implantation then optimizes the cable trays on the installation plan according to the previous calculations.
Cable management
Caneco Implantation enables the optimization of cable routing via junction boxes and cable trays.
It configures the cable selection rules for the trays.
It automatically produces cross-sectional views of your cable trays.
Publication of project documentation
Caneco Implantation enables you to edit all the documents of the project, i.e. nomenclatures for cables, terminal devices and cable trays, cable lists, cable schedules as well as lists of cable trays along with their cross section views.
Caneco Implantation automatically generates the cabling synoptic for LV and ELV installations.
Implantation of electrical equipment
Caneco Implantation main features include the implantation of electrical equipment in 2D/3D as well as the optimization of cable routing.
Caneco Implantation integrates a Low Voltage (LV) and Extra Low Voltage (ELV) object library that comprises distribution boards and cabinets, lighting features, specific and general purpose sockets outlets, cable trays, etc.
Caneco Implantation enables you to customize electrical equipment in the library and to add also symbols created in AutoCAD®.
Caneco Implantation allows you to import lighting features installed in Dialux® after the illumination calculations have been completed.
Sizing and calculations
The results are then re-imported into Caneco Implantation.