Caneco BIM
Revit® application for the design and control of a digital electrical model
Published by
ALPI
Caneco BIM
Published by
ALPI
Features
A digital collaborative platform
Caneco BIM main features include the exchange of electrical data between the Revit® digital model and the Caneco software range, automated cable management and sizing of electrical installations. Caneco BIM performs the exchange of electrical data between Revit®, and the rest of Caneco software range: Caneco BT, Caneco Implantation and Office Elec.
Automated cable management
Caneco BIM provides circuits creation tools
Its interface manages physical representation of cables inside Revit® allowing also the edition of circuit path
Caneco BIM performs cable routing management according to cable trays service types
Sizing of an electrical installation
Caneco BIM enriches the digital model with the results of calculations carried out in Caneco BT, such as cable cross-sections, protective devices and short-circuit currents.
It allows you to import all the technical documents into your Revit® project.
Caneco BIM updates cable trays inside Revit®
Complementary applications
Additional tools will help you control and validate your electrical installation in your model.
Caneco BIM allows the import of the cable types, as they are described in Caneco BT, directly into Revit®.
It analyses the objects and groups of objects and adds electrical parameters such as voltage, apparent load, load class etc.
Integrated electrical calculation boxes
Caneco BIM calculates the consumption of motors and lighting
Caneco BIM converts electro-technical units
It also calculates the reactive power of condenser batteries
A digital collaborative platform
Caneco BIM main features include the exchange of electrical data between the Revit® digital model and the Caneco software range, automated cable management and sizing of electrical installations. Caneco BIM performs the exchange of electrical data between Revit®, and the rest of Caneco software range: Caneco BT, Caneco Implantation and Office Elec.
Automated cable management
Sizing of an electrical installation
Caneco BIM updates cable trays inside Revit®