EcoStruxure™ Fire Expert
Published by
Schneider Electric
Features
Library of different features
EcoStruxure™ Fire Expert is an online application for efficient management of fire detection system. EcoStruxure™ Fire Expert application can receive data from different Esmi Sense FDP detection systems to remotely monitor and control these sources efficiently using one application. Users can sign in to the system and start to use selected features.
In EcoStruxure™ Fire Expert there is a library of different features. Each feature is licensed and can be bought complemented or combined with a previous license. Licenses are annual and assigned either to users or to fire detection systems.
Library of different features
EcoStruxure™ Fire Expert is an online application for efficient management of fire detection system. EcoStruxure™ Fire Expert application can receive data from different Esmi Sense FDP detection systems to remotely monitor and control these sources efficiently using one application. Users can sign in to the system and start to use selected features.
In EcoStruxure™ Fire Expert there is a library of different features. Each feature is licensed and can be bought complemented or combined with a previous license. Licenses are annual and assigned either to users or to fire detection systems.
In EcoStruxure™ Fire Expert there is a library of different features. Each feature is licensed and can be bought complemented or combined with a previous license. Licenses are annual and assigned either to users or to fire detection systems.