SQL4automation

Connect Programmable Logic Controllers to SQL databases
Published by Inasoft Systems GmbH

Features

  • Configuring connector service
  • Easy to use configuration tool
  • Debugger tool
  • Query tool
  • Data management
  • Multiple editions offered for users

Configuring connector service

The SQL4automation Connector runs as a lightweight service in the background and can be installed on Windows and Linux systems. It can be easily configured using the Configuration Tool.
Configuring connector service

Easy to use configuration tool

With the S4A-Config Tool you can set up and test database connections. It shows an overview of all connections and allows you to configure your links. The Config Tool can be installed alongside the connector, or on a different device in the same network.
Easy to use configuration tool

Debugger tool

The S4A-Debugger is an extensive diagnoses tool for all type of reports. It records all connections and highlights false SQL queries as well as queries which do not return any values. This greatly facilitates the troubleshooting, saves valuable commissioning time and reduces downtimes and idle times. The Debugger can be installed alongside the connector, or on a different device in the same network.
Debugger tool

Query tool

The S4A-Query-Tool tests the connection between the Connector and the database as well as the SQL commands. As soon as a SQL command is correct it can be copied to the controller via Ctrl+C Ctrl+V. This enables you to speed up the development and testing of your requests. The Query Tool can be installed alongside the connector, or on a different device in the same network.
Query tool

Data management

SQL4automation gives you many advantages over other existing solutions on the market.
Your advantages with SQL4automation:
  • The complete programming is done in the controller. The implementation of a middleware is not required.
  • The SQL4automation Connector is only parameterised: No additional project specific changes are necessary.
  • The controller is the master und determines when which data is written or read.
  • The controller gets the data directly from the database.
  • The performance is very high thanks to TCP/IP communication.
  • Only one interface for multiple controllers.
  • No OPC.

Multiple editions offered for users

As users will have multiple needs, we offer a variety of editions to suit your purpose.
  • Runs as a service
  • IP-Filter for target access
  • DB-Connection via ODBC
  • Debugger for Debugging
  • Query-Tool for Testing
  • Runs on Windows & Linux
  • Light - 750 Euro
    • In our Light version, a user has access to 1 Link (connects 1 PLC to 1 database).The amount of data is not limited.
    Standard - 980 Euro
    • In our Standard version, a user has up to 10 simultaneous connections (1 Link connects 1 PLC to 1 database), which can be established from one or more PLCs to one or more databases.The amount of data is not limited.
    Ultimate - n * 980 Euro
    • In our Ultimate version, a user has up to n times 10 simultaneous connections (1 Link connects 1 PLC to 1 database) which can be established from one or more PLCs to one or more databases. The amount of data is not limited.