RemoteConnect for the SCADAPack x70
Configuration & programming software application
Published by
Schneider Electric
RemoteConnect for the SCADAPack x70
Published by
Schneider Electric
Free
Features
Object database
User-defined names (tags):
Tags are easily understood, relating directly to the process and/or equipment, and functionality
RemoteConnect Object Browsers
Offline browser provides grouping, filtering, and sorting, for easy viewing and manipulation
Export/Import to/from Microsoft® Excel:
Save time with external editing and templating of configurations - particularly for large systems
Protocol-agnostic:
Associate Modbus registers, IEC 60870-5-104 objects, and/or DNP3 Level 4 objects with tagged database objects/variables
DNP3 data-concentrator Master for retrieval of DNP3 events and data
Modbus Scanner for configuration-based polling of Modbus devices
Exchange object information with Linux applications and IIoT protocols with the SCADAPack 47xi
Support for large object databases:
Up to 15000 objects with 6000 logic-connected objects
Up to 100,000 DNP3 or IEC 60870-5-104 Events
Logic editor
Share program sections with Modicon PLCs:
Logic code re-use between SCADAPack RTUs and Modicon PLCs
Supports all five IEC 61131-3 logic languages:
FBD – Function Block Diagram
LD – Ladder Diagram
SFC – Sequential Function Chart
IL – Instruction List
ST – Structured Text
Export/Import of logic program sections for reuse in other projects
Cybersecurity
IP Communications:
Use the IP Firewall to restrict inbound & outbound communications to specific IP addresses or IP ranges
Use the IP Firewall to Restrict communications to specific IP services or port numbers to limit access
Choose which IP services to enable/disable and when, thus limiting cyber attack-surface exposure
Ruggedized IP communications and RTU operations tested to comply with Achilles® Level 2 and Synopsis Defensics™
DNP3 SAv2 Secure Authentication:
Authentication of critical commands over DNP3
Security at the Edge with the SCADAPack 47xi
IEC 622443 SL1 compliant SCADAPack 47xi adds support for Network Address Translation (NAT)
Secure boot resists software-injection attacks by malware and a SCADAPack 47xi TPM helps to protect data stored on the device
Read-only Linux root file system provides infrastructure for user applications and extensions using Linux overlay file system technology
Use AppArmor™ with individual Linux applications and containers to develop and implement profiles and restrict access to only needed permissions and resources
Edge
SCADAPack 47xi supports edge solutions including:
IIoT and Internet protocols such as MQTT, Sparkplug B, OPC UA, SNMP, and REST API using tools such as Node-RED®
Automatically create SMS and email messages corresponding to alarms and other events based on remote site conditions
Integrated webserver and develop custom web applications
Development using general purpose languages such as C, C++, or Python
Development and deployment using container technology such as Docker™
Third-party device management
RemoteConnect is an FDT2 DTM Container
RemoteConnect accepts plug-in software DTMs of version 2 or version 1.2
Device DTMs are available from instrument vendors and provide an operator interface for managing and configuring the device
Communication DTMs provide the ‘protocol’ connection between the DTM and the device
Gateway DTMs act as a comms. bridge between networks and comm. DTMs
Object database
User-defined names (tags):
RemoteConnect Object Browsers
Export/Import to/from Microsoft® Excel:
Protocol-agnostic:
Support for large object databases:
Logic editor
Share program sections with Modicon PLCs:
Supports all five IEC 61131-3 logic languages:
Export/Import of logic program sections for reuse in other projects
Cybersecurity
IP Communications:
DNP3 SAv2 Secure Authentication:
Security at the Edge with the SCADAPack 47xi
Edge
SCADAPack 47xi supports edge solutions including:
Third-party device management
RemoteConnect is an FDT2 DTM Container