iVisionmax-Secure VMS Connector
DCS/PLC Alarm to Video Management System(VMS)
Published by
L&T Electrical & Automation

iVisionmax-Secure VMS Connector
Published by
L&T Electrical & Automation
Free
Editions & Pricing
Free Trial Version
Included
-
1 User
- The free trial for 30 days allows full features of the software
- Free version shall be provided for only one connection
Full version
$2,000.00
/ project
one time
For 1-10 Projects
$1,500.00
/ project
one time
For 11-25 Projects
$1,000.00
/ project
one time
For 26 Projects And Above
$200.00
/ additional connection
one time
For The First 31 Additional Connections
Included
-
1 User
- The software is available to customers at a one time price per project. In the customer's plant or site where one Control system(SCADA/DCS/BMS/PLC) and one VMS is deployed, our software will interface between the Control system and VMS as ONE project.
- Each project license comes with one interface/connection between control system(modbus/OPC) and VMS
-
Additional interfaces/connections for the same project is available to customers at the rate applicable per connection as above for a maximum of 31 interfaces
This additional interface is required if there are more than one control systems and/or VMS in the same project
- Setup is provided to customers free of charge for one day
- Post download of the software, the license would be sent to customer's email ID
Free Trial Version
Included
- 1 User
- The free trial for 30 days allows full features of the software
- Free version shall be provided for only one connection
Full version
For 1-10 Projects
For 11-25 Projects
For 26 Projects And Above
For The First 31 Additional Connections
Included
- 1 User
- The software is available to customers at a one time price per project. In the customer's plant or site where one Control system(SCADA/DCS/BMS/PLC) and one VMS is deployed, our software will interface between the Control system and VMS as ONE project.
- Each project license comes with one interface/connection between control system(modbus/OPC) and VMS
-
Additional interfaces/connections for the same project is available to customers at the rate applicable per connection as above for a maximum of 31 interfaces This additional interface is required if there are more than one control systems and/or VMS in the same project
- Setup is provided to customers free of charge for one day
- Post download of the software, the license would be sent to customer's email ID