pipe::scan for EcoStruxure™ WWW

Online waterquality monitoring sensor system
Published by scan Messtechnik GmbH

Features

  • Full-scale event detection
  • Hot-maintenance
  • Organics and Turbidity monitoring
  • Totally flow-independent
  • Accurate measurement
  • Low maintenance

Full-scale event detection

Full-scale event detection with real-time alarms within the drinking water distribution network. When an abnormal change occurs, the s::can event detection system sends an alarm to warn the operators.
Full-scale event detection

Hot-maintenance

Hot maintenance is possible as each sensor can be removed individually for maintenance without interrupting the flow or pressure. There is no need to shut down the whole pipe during maintenance.
Hot-maintenance

Organics and Turbidity monitoring

Complete suite of water quality parameters possible – everything you might want to measure in a network. We are able to measure colour, organics and turbidity as well as standard parameters. Identify potential hotspots and ensure discolouration is identified early, before it gets to the customers tap.
Organics and Turbidity monitoring

Totally flow-independent

Unique nanopump for sampling as nothing protrudes into the pipe and even works in stagnant conditions.
Totally flow-independent

Accurate measurement

Accurate measurement in perfect agreement to standardized lab reference... not just ”trending”.
Accurate measurement

Low maintenance

With a low power consumption and small footprint, the pipe::scan can be installed in almost any location, also in very remote areas. A 6 months service interval is sufficient to ensure a efficient, reliable stand-alone operation. This makes it perfect for drinking water network monitoring with multiple systems.
Low maintenance