SmartConnector OPC Classical Extension

OPC EBO middleware integration software
Published by LK Proekt Ltd.

Overview

Use third-party equipment in EcoStruxure™ Building easily!

SmartConnector OPC Classical Extension is set of libraries and configuration files, which can be integrated to the SmartConnector framework as extension. It supports the following OPC standards: OPC DA v2.05 and v3.00.


This software allows system integrators to acquire OPC data for EcoStruxure Building Operation even for big projects! It was tested on sites with more than 10 000 EWS variables (OPC tags).


Now it’s possible to connect any OPC DA server to enterprise server and standalone automation server. EBO integration and configuration are very easy thanks to automatically generated configuration files. The software gives possibilities to select required OPC tags and quickly adds them by UI configurator.


SmartConnector OPC Classical Extension requires SmartConnector framework version 2.3. and above. Please note that you will need a commercial license for SmartConnector from Schneider Electric.

Technology Partner

SmartConnector OPC Classical Extension

Main Window. OPC Servers Browsing

Adding tags to current configuration

Benefits

Free 30 days trial!

No limitations except 30 days! It means that you can install it on your project and make sure that everything works fine.

Reliability

The software works on more than twenty of our own sites. We have all the statistics about its operation, gathered over several years.

Saving time

Quick and simple configuration.