SmartConnector SNMP Extension

SNMP Manager for EcoStruxureâ„¢ Building Integration
Published by LK Proekt Ltd.

Features

  • Highlights
  • SNMP v1 v2 v3 supports
  • UI configurator
  • Custom MIB parsing
  • SNMP exchange monitoring

Highlights

High Capacity

Tested on up to 20.000 SNMP/EWS server variables capacity.

Software Requirements

SmartConnector SNMP Configurator software is tested on following operation systems:

  • Windows 7x64
  • Windows 10 x64
  • Windows Server 2008 x64
  • Windows Server 2012 x64
  • SNMP v1 v2 v3 supports

    EBO SNMP Manager Supports all versions of SNMP protocol.
    SNMP v1 v2 v3 supports

    UI configurator

    The software has a user-friendly interface that helps to work with SNMP entities easily.
    UI configurator

    Custom MIB parsing

    Users can add devices with custom MIB files, which is automatically parsed by the configurator.
    Custom MIB parsing

    SNMP exchange monitoring

    SNMP configurator allows monitoring data exchange by SNMP protocol and drops error messages when a communication failure occurs.