SmartConnector SNMP Extension
Overview
IT equipment monitoring in EcoStruxure™ Building
SmartConnector SNMP Extension allows EBO users, to monitor network devices via Simple Network Management Protocol (SNMP). It fits for really big projects! It was tested on up to 20.000 SNMP/EWS server variables capacity!
This software connector is an SNMP manager that obtains data from all required agents (servers) and includes a useful configurator, which allows creating the required configuration quickly.
SmartConnector SNMP Extension can be plugged into Schneider Electric SmartConnector Framework as an extension. SNMP Extension allows communicating between SNMP agents and EWS servers, corresponding to user-provided configuration. EWS server generates EBO alarms when TRAP-messages received. This extension supports the following versions of the SNMP protocol: v1, v2, v3.
SmartConnector SNMP Extension requires SmartConnector framework
version 2.3. and above. Please note that you will need a commercial license for SmartConnector from Schneider Electric.
IT equipment monitoring in EcoStruxure™ Building
SmartConnector SNMP Extension allows EBO users, to monitor network devices via Simple Network Management Protocol (SNMP). It fits for really big projects! It was tested on up to 20.000 SNMP/EWS server variables capacity!
This software connector is an SNMP manager that obtains data from all required agents (servers) and includes a useful configurator, which allows creating the required configuration quickly.
SmartConnector SNMP Extension can be plugged into Schneider Electric SmartConnector Framework as an extension. SNMP Extension allows communicating between SNMP agents and EWS servers, corresponding to user-provided configuration. EWS server generates EBO alarms when TRAP-messages received. This extension supports the following versions of the SNMP protocol: v1, v2, v3.
SmartConnector SNMP Extension requires SmartConnector framework version 2.3. and above. Please note that you will need a commercial license for SmartConnector from Schneider Electric.