Antisurge Control Application

Integrated antisurge control for compressors

Features

  • Highlights

Highlights

Fallback strategy
Continued and stabilized compressor running when one or more of the measurements are used for protection fail.

Performance deviation monitoring
Compressor performance deviation monitoring by ACA, flagging an alarm when the actual performance of the compressor deviates too much from the compressor performance curve that is stored in the ACA.

Load sharing
Load-balance compressor trains running in parallel and/or in series by adding our Station Control Application (SCA). This will add an algorithm for load sharing of compressors, both in parallel and in series.