X-Force E-Logbook

Digitization and automation software for industrial logbooks

Features

  • Easy to use
  • Simplified logs and data visualization
  • Time & location bound accuracy
  • Reporting and analytics as per your standard
  • Enterprise scalability
  • Advanced workflow visualisation
  • Real time process monitoring with situation awareness
  • Fast & accurate shift handover process
  • Integration with other IT/OT systems
  • Notifications & alerts

Easy to use

X-Force E-Logbook has very simple user interface in terms of complex activities like operational data entry, past data verification in real time, remarks, incident report, quick report mailing.
Easy to use
Zone specific tablets for mobile operations
  • X-Force E-Logbook can be implemented on zone specific industrial tablets for mobile operations.
Create workflow easily
  • X-Force E-Logbook has very simple and quick configurations like user creation, role assignment, job creation, job assignment, schedule generation, reports on demand.

Simplified logs and data visualization

E-Logbook provides great visualization of data in the form you need. It provides most sophisticated trending view experience with features like real time trending, historical trending, multi parameter trending, trend export etc.
Simplified logs and data visualization

Time & location bound accuracy

With the features like location lock and time bound X-Force E-Logbook can guarantee unfabricated data entries from correct location on correct time.
Time & location bound accuracy
Ensuring operator going to specific location for log data entry
  • X-Force E-Logbook solution is enabled with wifi, RFID, and GPS services to ensure that operator is going to field or not. Also the application enforces the user to follow the configured schedule on time.

Reporting and analytics as per your standard

X-Force E-Logbook is a customized solution which can be developed according to client's reporting and analytics requirement.

Reporting options: real-time report, dashboards, live table and more.
Reporting and analytics as per your standard

Enterprise scalability

X-Force E-Logbook can integrate every aspect of industrial operations from multiple processes to multiple manufacturing division located across world. All of this with seamless real time visualization.
Enterprise scalability

Advanced workflow visualisation

X-Force E-Logbook provides powerful workflow management which takes care of multiple roles and users with suitable rights and single click approvals.
Advanced workflow visualisation

Real time process monitoring with situation awareness

X-Force E-Logbook has features like image / video visualization for exact situation awareness along with step by step process execution tracking. With the help of integration with RFID / NFC X-Force E-Logbook has assured accurate situation awareness.
Real time process monitoring with situation awareness

Fast & accurate shift handover process

We are aware that shift handover happens 3 times every day which is very important transaction of information between two teams or operators. Also shift handover are prone to miscommunication, misunderstanding and other human errors.
Our solution nullifies the possibilities of errors during shift handover as X-Force E-Logbook provides complete shift handover solution by cross checking important parameters with real time updates which assures efficient communication.

Integration with other IT/OT systems

X-Force E-Logbook can be integrated with various ERP systems like SAP, Oracle, Microsoft Dymanics etc. It also communicates flawlessly with major historians, databases like SQL and other control system components like DCS, PLC or SCADA.

Notifications & alerts

Along with auto mailing, scheduled reports and reports on demand X-Force E-Logbook can provide important notification for incorrect data entry based on predefined set points.