EcoStruxure™ Control Expert - Liquid Food Library

Control modules focused on the needs of the liquid food process
Published by Schneider Electric

Overview

EcoStruxure™ Control Expert - Liquid Food Library
The liquid food library had been in existence since 2013 and was extended in 2016 to support Wonderware System Platform. It provides customers access to automation logic for Ecostruxure™Control Expert (Modicon Controllers) and objects Wonderware System Platform, as well as the market leading software portfolio of Aveva for Food & Beverage applications.

EcoStruxure™ Control Expert - Liquid Food Library

Operation

Benefits

Wonderware System Platform
Wonderware Software (AVEVA) is the standard for liquid food applications. This library provides pre-built capabilities for Ecostruxure™ Control Expert and System Platform 2014 (and above).
Situational awareness
The Library is based on Situational Awareness concepts. This helps operators identify states that are different from the expected and from the normal operating mode.
Control modules
The Liquid Food Library provides control modules which are focused on the needs of the liquid food process : Multi-Directional Valves (2-way, 3-way & 4-way), Mix Proof Valves and Cyclical Motors.
Instrumentation
The Liquid Food Library provides control modules which are focused on the needs of the liquid food process : Weighing Systems (Scaime) , Custodial Flow Measurement and Milk Analyzers.
Processes
The Liquid Food Library provides control modules which are focused on the needs of the liquid food process : S88/NS88 Sequence Management, Line Reservation and CIP Recipes.