Hybrid DCS Template Library for Electrical Motors with Conventional Starters
Motor templates with local/remote selection
Published by
SUPERTECH INSTRUMENTATION SERVICE

Hybrid DCS Template Library for Electrical Motors with Conventional Starters
Published by
SUPERTECH INSTRUMENTATION SERVICE
Free Trial
Features
Highlights
This HDCS template library consists of the following 3 templates which can be used with Schneider Electric EcoStruxure™ Hybrid DCS for automation in batch and continuous process applications, typically in specialty chemicals, consumer products, food & beverages and pharma industries.
Compatible with: EcoStruxure™ Hybrid DCS R2 and onwards
Electrical Motor Template (3DI, 1DO)
-
This template is similar to “$Motor” template available in the HDCS General Purpose Library. In the original template, motor is turned on even in the simulation mode. Local/remote switch is considered in the MCC panel or field. In our template, motor is not turned on in the simulation mode.
Electrical Motor Template with Local / Remote Selection (2DI, 2DO)
-
This template is similar as the previous template. Additionally, this template has a provision for local/remote selection from the DCS by a soft switch.
Electrical Motor Template with Feeder Functionality (6DI, 2DO)
-
This template provides additional feeder information, such as feeder power-on and other permissive for interlocking like Emergency push-button feedback.
Hardware platform compatibility
-
This HDCS Template library is compatible with the following hardware platforms:
- - Quantum
- - Premium
- - M340
- - M580
Highlights
This HDCS template library consists of the following 3 templates which can be used with Schneider Electric EcoStruxure™ Hybrid DCS for automation in batch and continuous process applications, typically in specialty chemicals, consumer products, food & beverages and pharma industries.
Compatible with: EcoStruxure™ Hybrid DCS R2 and onwards
Electrical Motor Template (3DI, 1DO)
- This template is similar to “$Motor” template available in the HDCS General Purpose Library. In the original template, motor is turned on even in the simulation mode. Local/remote switch is considered in the MCC panel or field. In our template, motor is not turned on in the simulation mode.
Electrical Motor Template with Local / Remote Selection (2DI, 2DO)
- This template is similar as the previous template. Additionally, this template has a provision for local/remote selection from the DCS by a soft switch.
Electrical Motor Template with Feeder Functionality (6DI, 2DO)
- This template provides additional feeder information, such as feeder power-on and other permissive for interlocking like Emergency push-button feedback.
Hardware platform compatibility
-
This HDCS Template library is compatible with the following hardware platforms:
- - Quantum
- - Premium
- - M340
- - M580