Hybrid DCS Template Library - Sequencer for Batch Processes

Template library for sequential batch process operations up to 64 steps with operator messages

Features

  • Highlights

Highlights

This HDCS Template library consists of sequencer template which can be used with Schneider Electric EcoStruxureâ„¢ Hybrid DCS for automation in batch and continuous process applications, typically in specialty chemicals, consumer products, food & beverages and pharma industries.

Compatible with: EcoStruxureâ„¢ Hybrid DCS R2 and onwards

This Sequencer template provides the following functionalities
  • The sequence of operations can be carried out in either auto mode or manual mode.
  • The template is designed for processes sequence up to 64 steps and 5 parameters control.
  • The Individual steps progress from one step to the other consecutive step depending upon the predefined logic conditions.
  • The template provides informative and operator friendly sequence control with operator guide message feature.
  • Sequence step can be edited with add, edit and delete.
  • The template provides facility to store one sequence for each instance.
Hardware platform compatibility
  • This HDCS Template library is compatible with the following hardware platforms:
  • - Quantum
  • - Premium
  • - M340
  • - M580
Unauthorised background image

Your product is just steps away!

Register for FREE to buy, get downloads and access free trials.

Get Resources and Start FREE Trials

Easy Product Activation with Your Account

Products Saved to Personal Digital Library