Hybrid DCS Template Library - Sequencer for Batch Processes

Template library for sequential batch process operations up to 64 steps with operator messages

Overview

Sequencer Template for Batch Processes

This template library consists of a customized template for sequential process operations in batch processes widely used in process industries. The template provides the following functionalities:

  • Define up to 64 steps for commonly used processes
  • Provide operators with guide messages for each step
  • Access to recipe editor
  • Define up to 5 parameters control
  • Supertech is a leading Automation Solution Provider with more than 30 years of experience in a wide range of process industries. We are Alliance Integration Partners with Schneider Electric for their Automation Products (PLC, SCADA, DCS, VFDs & Soft-starters, and Intelligent MCCs) and EcoXpert for Energy Monitoring Solutions.

    Hybrid DCS Template Library - Sequencer for Batch Processes

    Benefits

    Save time

    This library maintains the project standardization. Its pre-configured template reduces the engineering efforts to about 75%.

    Decrease in error

    This library has thoroughly tested template which results in 90% decrease in errors.

    Ready to use

    This library is ready to use for controller based batch operation with fixed recipes up to 64 steps (auto/semi-auto/manual modes of operation possible). All batch events and operator actions are automatically logged in DCS. It's easy to configure and user friendly operation.

    Fully tested

    This template library comes with fully tested and verified DCS template for sequencer.