Hybrid DCS Template Library for Automated On-Off Valves

Template library for pneumatic actuated valve, two stage valve and motorized valve

Features

  • Highlights

Highlights

This HDCS Template Library for Automated On-Off Valves consists of the following 3 templates. These can be used with Schneider Electric EcoStruxure™ Hybrid DCS for automation in batch and continuous process applications, typically in specialty chemicals, consumer products, food & beverages and pharma industries.

Compatible with: EcoStruxure™ Hybrid DCS R2 and onwards
On-off valve template with pneumatic actuator (2DI, 1DO)
  • This template is similar to the “$Valve” template available in the HDCS General Purpose Library. In the original template, the output is generated even in the simulation mode, which is not desired. With our template, there is no output change in the simulation mode.
Two-stage on-off valve template with pneumatic actuator (3DI, 2DO)
  • It is a common practice to use two-stage valves for accurate charging of liquid raw materials. For example, when 95% (or as per the requirement) of the material is transferred, the valve closes to about 10% (or as per the requirement). In case for the complete material transfer, the valve closes completely.
Motor operated valve template (10DI, 3 DO)
  • This template is used for motor operated on-off valves, which are used in water, wastewater and many other applications.
Hardware platform compatibility
  • This HDCS Template Library is compatible with the following hardware platforms:
  • - Quantum
  • - Premium
  • - M340
  • - M580