SEE Electrical

Electrical CAD software
Published by IGE+XAO

Overview

SEE Electrical

Create electrical schematics with SEE Electrical in a few clicks. All features and commands in SEE Electrical are designed specifically for electrical engineering. Its intuitive interface means that you can be productive very quickly with minimal training.


SEE Electrical can be accesed in three levels - Basic, Standard and Advanced - via download. Each offers a range of services at a different price point so that you can select the level that suits your needs. It is simple to progress from one level to another, as you can work on project data across all levels simultaneously.

SEE Electrical

SEE Electrical V8R2

Benefits

Intuitive
SEE Electrical intuitive interface means that you can be productive very quickly, with minimal training. Creating wiring diagrams has never been so simple!
Flexible
Simply selected one of the 3 plans available, and be on your way to creating wiring diagrams.