CYPELEC Core
Published by
CYPE
Overview
Design of low voltage electrical installations.
CYPELEC Core is a program for the design of low-voltage electrical installations. Users can draw single-line diagrams of the installation and configure the properties of the elements it contains.
CYPELEC Core is a free application and can be downloaded exclusively from the BIMserver.center® platform. The current version can be installed in either Spanish, or Catalan. More languages to be made available in upcoming versions.
Design of low voltage electrical installations.
CYPELEC Core is a program for the design of low-voltage electrical installations. Users can draw single-line diagrams of the installation and configure the properties of the elements it contains.
CYPELEC Core is a free application and can be downloaded exclusively from the BIMserver.center® platform. The current version can be installed in either Spanish, or Catalan. More languages to be made available in upcoming versions.