CYPELEC Core
Published by
CYPE
Features
Highlights
Our solution has functionalities for the load flow and short circuit design, allowing users to edit all the elements with no restrictions on the power or number of lines. Its results output allows users to obtain drawings of the single-line diagram, justification reports, quantity and results table.
The design checks carried out in the program are based on the specifications of the international IEC standards.
This application is integrated in the Open BIM workflow using the IFC standard, and so maintains the interaction with the rest of the tools.
Highlights
Our solution has functionalities for the load flow and short circuit design, allowing users to edit all the elements with no restrictions on the power or number of lines. Its results output allows users to obtain drawings of the single-line diagram, justification reports, quantity and results table.
The design checks carried out in the program are based on the specifications of the international IEC standards.
This application is integrated in the Open BIM workflow using the IFC standard, and so maintains the interaction with the rest of the tools.